sns_ctx

Outline

Reference contexts.

C format

 BOOL    sns_ctx (void);
Parameter(s)

None.

Explanation

This service call examines the context type of the processing program that issues this service call. This service call returns TRUE when the processing program is non-task context, and return FALSE when the processing program is task context.

Return value

Macro

Value

Description

TRUE

1

Normal completion (non-task context).

FALSE

0

Normal completion (task context).

E_CTX

-25

Context error.

- This service call was issued in the status PSW.IPL > kernel interrupt mask level.