sns_loc

Outline

Reference CPU locked state.

C format

 BOOL    sns_loc (void);
Parameter(s)

None.

Explanation

This service call examines whether the system is in the CPU locked state or not. This service call returns TRUE when the system is in the CPU locked state, and return FALSE when the system is in the CPU unlocked state.

Return value

Macro

Value

Description

TRUE

1

Normal completion (CPU locked state).

FALSE

0

Normal completion (CPU unlocked state).

E_CTX

-25

Context error.

- This service call was issued in the status PSW.IPL > kernel interrupt mask level.