< Assembler Command Options / Source Options >
[Format]
-define=<sub>[,...]
<sub>: <macro name> = <string>
|
[Description]
- | This option replaces the macro name with the specified string.
(This provides the same function as writing the .DEFINE directive at the beginning of the source file.)
|
[Remarks]
- | .DEFINE takes priority over the define option if both are specified. |