-chkdpfpu [V3.01.00 or later]


< Assembler Command Options / Source Options >

[Format]

-chkdpfpu

[Description]

-

This option outputs warning W0551017 when a double-precision floating-point processing instruction is written in the source file.

[Remarks]

-

For details of the double-precision floating-point processing instructions, refer to the RX Family Software Manual.