< Optimizing Linkage Editor (rlink) Options / List Options >
If no list file name is specified, a list file with the same name as the output file (or first output file) is created, with the extension lbp when form=library or extract is specified, or map in other cases. |
Even if the section allocation address exceeds the allowable address range, this option outputs the link map information and symbol information. In this case, "**OVER**" is output. [V2.06.00 or later] |