< Optimizing Linkage Editor (rlink) Options / List Options >
-show [=<sub>[,...]] <sub>:{ symbol | reference | section | xreference | total_size | vector | struct | relocation_attribute | all} |
Table 2.17 lists the suboptions. |
The following table shows whether suboptions will be valid or invalid by all possible combinations of options form, show, and/or show=all. |
When optimization is specified at compilation, information about branches to immediate subordinate functions is not output. |
When optimization of access to external variables is specified, information about references to variables other than base symbols is not output. |
When show=reference is valid, the number of references of the variable specified by #pragma address is output as 0. |