< Optimizing Linkage Editor (rlink) Options / Optimize Options >
[Format]
-optimize [= <suboption>[,...] ]
<suboption>: { SYmbol_delete | SAMe_code | SHort_format | Branch | SPeed | SAFe }
|
When this option is omitted, the default is optimize.
[Description]
- | When optimize is specified, optimization is performed for the file specified with the goptimize option at compilation or assembly. |
- | -optimize (no suboptions) executes all optimization. It has the same meaning as
-optimize=symbol_delete,same_code,short_format,branch.
|
- | -optimize=speed executes optimizations other than those reducing object speed. It has the same meaning as
-optimize=symbol_delete,short_format,branch
|
- | -optimize=safe executes optimization other than those limited by variable or function attributes. It has the same meaning as -optimize=short_format,branch |
- | Other suboptions mean optimization as the following table. |
Table 2.18 | Suboptions of optimize Option |
|
|
|
|
|
symbol_delete
|
Deletes variables/functions that are not referenced.
Always be sure to specify #pragma entry at compilation or the entry option in the optimizing linkage editor.
|
O
|
X
|
same_code
|
Creates a subroutine for the same instruction sequence.
|
O
|
X
|
short_format
|
Replaces an instruction having a displacement or an immediate value with a smaller-size instruction when the code size of the displacement or immediate value can be reduced.
|
O
|
O
|
branch
|
Optimizes branch instruction size according to program allocation information. Even if this option is not specified, it is performed when any other optimization is executed.
|
O
|
O
|
Notes 1. | RXC: C/C++ program for RX Family,
RXA: Assembly program for RX Family
|
[Remarks]
- | When form={object | relocate | library} or strip is specified, this option is unavailable. |
- | When a start function with #pragma entry or entry is not specified, optimize=symbol_delete is invalid. |