< Optimizing Linkage Editor (rlink) Options / Optimize Options >
Disables optimization for the specified section. If an input file name or library module name is also specified, the optimization can be disabled for a specific file, not only the entire section. |
To disable optimization for an input file with its path name, type the path with the file name when specifying section_forbid. |