2.1 Overview
The resource information tool can be used to confirm the RI600PX resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
The operating procedures for the resource information tool are described below.
Launch the CubeSuite+ from the [start] menu of Windows.
Remark See "CubeSuite+ Start" for details on "Start CubeSuite+".
Open the project to debug.
Remark See "CubeSuite+ Start" for details on "Open project".
Select the type of debugging tool with which to debug the program (E1, E20 or Simulator).
Remark See "CubeSuite+ RX Debug" for details on "Select debug tool".
Download the program to debug.
Remark See "CubeSuite+ RX Debug" for details on "Download programs".
Remarks 1. When a program using the RI600PX functionality is downloaded, this panel opens automatically.
2. The value will be indeterminate for the RI600PX resource information shown when the RI600PX system initialization is incomplete, because it will not be managed by the RI600PX.
(6) Execute/stop programs
Run the program to the location for which you wish to display the RI600PX resource information.
Remark See "CubeSuite+ RX Debug" for details on "Execute/stop programs".