Realtime OS Resource Information panel
 | 
 This panel displays the RI600PX resource information (e.g. system information and memory area information) of the RI600PX.
 
 Figure A-1.    Realtime OS Resource Information Panel
 
 The following items are explained here.
 
 -	 From the [Debug] menu, select [Download].
 
 -	 From the [View] menu, select [Realtime OS] >> [Resource Information].
 
 [Description of each area]
 
 This panel has the following tabs:
 
 (2)	 Information display area
 
 This area displays the RI600PX resource information (e.g. system information and memory area information) of the RI600PX.
 
 Remark	 A non-existent state of the resource is supported in RI600PX. Therefore, 
"--" is displayed by resource information when a resource is non-existent.