[Mutex] tab

This tab displays the mutex information (e.g. Mutex Name and ID) of the RI600PX.

Figure A-17. [Mutex] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

(a) First layer

This layer displays the mutex information (e.g. Mutex Name and ID) of the RI600PX.

This layer consists of the following items.

Mutex Name

An icon indicating the current status of the mutex and the name of the mutex are shown in the following format.

Icon Name

There are waiting tasks.

There are no waiting tasks. (The task locking the mutex)

There are no waiting tasks.

Non-existent mutex

ID

The ID of the mutex is shown.

Queue Status

The current status of the mutex is shown.

Waiting Tasks

There are waiting tasks.

Empty

There are no waiting tasks.

Locking Task ID

The ID of the locking task is shown.

Attribute

The attributes of the mutex is shown.

TA_CEILING

Priority ceiling protocol

Ceiling Priority

The ceiling priority of the mutex is shown.



(b) Second layer

The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the mutex's wait queue.

See the [Task] tab for details about waiting task information.

Figure A-18. [Mutex] Tab (Waiting Task Information)



[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Mutex Name, ID, Queue Status, Locking Task ID, Attribute, Ceiling Priority

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

ID, Locking Task ID, Ceiling Priority

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Reset Display Item

Resets the item displayed to initial state.