|
Detailed Settings of Timer Measurement dialog box [E1] [E20] [EZ Emulator]
|
This dialog box is used to display and change the detailed information on the timer event selected on the Events panel. Note that you cannot edit the address value of the timer event in this dialog box. If you need to edit the address value, first delete the timer event and then create a new one. For details on timer event setting, see "2.14 Measuring the Execution Time".
Figure A.41 | Detailed Settings of Timer Measurement Dialog Box |
This section describes the following.
[How to open]
- | On the Events panel, move the caret to the timer event of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu. |
[Description of each area]
(1) | Detailed information display/change area |
In this area, detailed information on the timer event selected in the Events panel is displayed by category in the list. Also, you can directly change its settings.
(2) | Property description area |
In this area, brief description of the categories and properties selected in the detailed information display/change area is displayed.
[Toolbar]
|
|
Displays categories in the detailed information display/change area.
|
|
|
Hides categories in the detailed information display/change area and rearranges only property items in the ascending order.
|
[Description of each category]
You can display and modify the detailed settings on timer measurement.
|
Measurement item Note
|
Specify the measurement item.
Displays "Execution cycle".
|
|
Default
|
Execution cycle
|
|
Modifying
|
Select from the drop-down list
|
|
Available values
|
One of the following as selected from the drop-down list.
[RX600, RX700 Series]
Execution cycle, Execution cycle (Supervisor mode), Exception and interrupt cycle, Exception cycle, Interrupt cycle, Execution count, Exception and interrupt count, Exception count, Interrupt count
[RX200 Series]
Execution cycle
|
|
Execution only once
|
Specifies whether to end the measurement after measuring the specified segment only once.
|
|
Default
|
No
|
|
Modifying
|
One of the following as selected from the drop-down list
|
|
Available values
|
Yes
|
Ends the measurement after measuring the specified segment only once.
|
|
No
|
The measurement value is cumulated every time you pass through the specified segment.
|
Note | [RX100 Series]
These microcontrollers does not support timers. |
[Function buttons]
|
|
|
|
OK
|
Applies the detailed settings specified in the dialog box to the timer event and closes this dialog box.
|
|
Cancel
|
Nullifies settings and closes this dialog box.
|
|
Help
|
Displays the help for this dialog box.
|