Go to the Location dialog box


Move the caret to a specified position.

Figure A.48

Go to the Location Dialog Box

 

This section describes the following.

[How to open]

-

Choose [Go To…] from the [Edit] menu.

-

On the Disassemble panel, select [Go To…] on the context menu.

-

On the IOR panel, select [Go To…] on the context menu.

[Description of each area]

(1)

[Address/Symbol] or [IOR] area

Specify a location to which you want the caret to be moved.

Enter directly in the text box (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).

The content of specification differs with the panel concerned, as shown below.

Subject panel

Content of specification

Disassemble panel

Address expression

IOR panel

I/O register name

Remark

If this dialog box is opened from the Disassemble panel by pressing the [Ctrl] + [Space] keys in the text box here, it is possible to complement a symbol name at the current caret position (see "2.21.2 Symbol name completion function").

[Function buttons]

Button

Function

OK

Moves the caret to the subject panel, with a specified position appearing at the beginning of display.

Cancel

Nullifies settings and then closes this dialog box.

Help

Displays help for this dialog box.