2.6.2 Displaying the disassembled result

To display the disassembled result (disassembled text) of a downloaded program (memory content), use the Disassemble panel shown below.

Choose [Disassemble] from the [View] menu and then select [Disassemble1 - 4].

Up to four disassemble panels can be opened at a time, with each panel discriminated by the name in their title bar, "Disassemble1," "Disassemble2," "Disassemble3," or "Disassemble4."

For details on how to read each area and details about their functionality, see the section in which the Disassemble panel is described.

Figure 2.90

Displaying the Disassembled Result (Disassemble Panel)

Remark

In the Scroll Range Settings dialog box which opens by clicking on [View] >> , in the toolbar, you can set the scroll range of the vertical scroll bar on this panel.

 

Following methods of operation are described here.

 

2.6.2.1 Changing the display mode

2.6.2.2 Changing the display form

2.6.2.3 Moving to a specified address

2.6.2.4 Moving to a symbol definition part

2.6.2.5 Saving the displayed contents of disassembled results