Renesas Electronics
The instructions and instruction codes displayed on the Disassemble panel can be edited (line-assembled).
Following methods of operation are described here.
2.6.4.1 Editing instructions
2.6.4.2 Editing instruction code