[Pin Number] tab


This tab displays information on each pin of the microcontroller in the order of pin number.

Figure A.8

[Pin Number] Tab

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View].

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then press the [Enter] key.

-

From the [View] menu, select [Code Generator 2] >> [Device List View].

[Description of each area]

(1)

Device list view area

This area displays the “device list view” for entering information on the pins of the microcontroller.

The device list view in this area is organized in the order of pin number.

The following are the columns comprising the device list view.

Pin no.

Displays the pin number of the pin.

Pin name

This area allows you to select “which function to use” when the pin has more than one functions.

Pin function

Displays the summary of function of the pin.

Pin direction

Displays the pin direction of the pin.

Pin remarks

Displays the precaution on using the pin.

Comment

(maximum 200 characters)

Displays the comment of the pin

Comments can be arbitrarily set up by 200 characters or less