This tab displays information on each pin of the microcontroller in the order it was grouped into peripheral functions.
The following items are explained here.
On the Project Tree panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View].  | 
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then press the [Enter] key.  | 
This area displays the “device list view” for entering information on the pins of the microcontroller.
The device list view in this area is organized in the order the pins were grouped into peripheral functions.
The following are the columns comprising the device list view.