This class creates a pseudo-error condition. [RH850][E1/E2/E20/Full-spec emulator/IE850A]
Specify the name (abbreviated form) of the error to be generated as a pseudo-error. See the debugger.PseudoError.Get function for the name (abbreviated form) of the error that can be specified. |
|
Specify the name of the IOR bit that will generate a pseudo-error. See the debugger.PseudoError.Get function for the name of the IOR bit that can be specified. |
|
Specify the address to be stopped the program after generating a pseudo-error as a list. |
"PseudoErrorCondition" is in class format, and the pseudo-error condition is set in the variable. |