BankedRegisterInfo


This class holds information on the save register bank (return value of the debugger.SaveRegisterBank.Information function). [RX]

[Type]

class BankedRegisterInfo:
        BankNumber = ""
        RegisterName = ""
        Value = ""

[Variable]

Variable

Description

BankNumber

This holds the bank number.

RegisterName

This holds the name of the register.

Value

This holds the value.

[Detailed description]

-

BankedRegisterInfo is a class, and it is passed as the return value when the debugger.SaveRegisterBank.Information function is executed.

[Example of use]

>>> srb = debugger.SaveRegisterBank.Information([1, 3])
 
Save register bank 1
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
Save register bank 3
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
--------------
>>> print srb[0].BankNumber
1
>>> print srb[0].RegisterName
R1
>>> print srb[0].Value
0