This class holds result information of the action event (return value of the debugger.ActionEvent.Get function).
[Type]
class ActionEventInfo:
Number = 0
Name = ""
Address = ""
Output = ""
Expression = ""
ActionEventType = ActionEventType.Printf
HostDate = ""
|
[Variable]
|
|
|
|
Number
|
This holds the action event number (numerical value).
|
|
Name
|
This holds the name of the action event (string).
|
|
Address
|
This holds the address of the action event.
|
|
Output
|
This holds the string to be attached at output.
|
|
Expression
|
This holds the variable expression (string).
|
|
ActionEventType
|
This holds the type of the action event.
|
|
|
|
|
ActionEventType.Printf
|
Printf event
|
|
HostDate
|
This holds the time in the host PC when an action event occurred.
Take account of the time being that in the host PC.
|
[Detailed description]
[Example of use]
>>>ae = ActionEventCondition()
>>>ae.Address = "main"
>>>ae.Output = "result "
>>>ae.Expression = "chData"
>>>ae.ActionEventType = ActionEventType.Printf
>>>ae_number = debugger.ActionEvent.Set(ae)
:
>>>out = debugger.ActionEvent.Get()
result chData=0x64
result chData=0x65
result chData=0x66
>>>print out[0].Address
main
|