This class creates conditions of the download file (parameters of the debugger.Download.Property property).
[Type]
class DownloadCondition:
FileName = ""
DownloadFileType = DownloadFileType.LoadModule
DownloadObject = True
DownloadSymbol = True
VendorType = VendorType.Auto
OutputInputCorrection = True
|
[Variable]
|
|
|
|
FileName
|
Specify the full path of the download file.
|
|
DownloadFileType
|
Specify the type of the download file.
The types that can be specified are shown below.
|
|
|
|
|
DownloadFileType.LoadModule
|
Load module file (default)
|
|
DownloadFileType.Hex
|
Intel HEX file
|
|
DownloadFileType.SRecord
|
Motorola S-record file
|
|
DownloadFileType.Binary
|
Binary file
|
|
DownloadObject
|
Specify whether to download object information.
True: Download object information.
False: Do not download object information.
|
|
DownloadSymbol
|
This holds whether to download symbol information.
True: Download symbol information.
False: Do not download symbol information.
|
|
VendorType
|
Specify the vendor of the compiler.
The types that can be specified are shown below.
|
|
|
|
|
VendorType.Auto
|
Automatically specify the vendor of the compiler judging from the output contents of debugging information (default).
|
|
VendorType.Ghs
|
Make this specification when using a compiler made by Green Hills Software, Inc.
|
|
OutputInputCorrection
|
Specify whether to generate information for the input correction feature.
True: Generate information for the input correction feature.
False: Do not generate information for the input correction feature.
|
[Detailed description]
[Example of use]
>>>di = debugger.Download.Property
>>>print di[0].FileName
C:\project\test.abs
>>>print di[0].DownloadFileType
LoadModule
>>>dc = DownloadCondition()
>>>dc.FileName = "C:/project/test2.abs"
>>>dc.DownloadFileType = DownloadFileType.LoadModule
>>>di.Add(dc)
>>>debugger.Download.Property = di
>>>
|