This function sets a conditional trace.
[Specification format]
debugger.Trace.Set(TraceCondition)
|
[Argument(s)]
|
|
|
|
TraceCondition
|
Specify a condition of a conditional trace.
See the TraceCondition class for creating a conditional trace.
|
[Return value]
Set trace event number (numerical value)
[Detailed description]
- | This function sets a conditional trace according to the contents specified with TraceCondition. |
- | The specified conditional trace is registered with the following name. |
[Example of use]
>>>tc = TraceCondition()
>>>tc.StartAddress = "main"
>>>tc.EndAddress = "chData"
>>>tc.EndData = 0x20
>>>tc.EndTraceType = TraceType.Write
>>>ts_number = debugger.Trace.Set(tc)
1
>>>print ts_number
1
|