|
debugger.ActionEvent.Information
|
This function displays action event information.
[Specification format]
debugger.ActionEvent.Information()
|
[Argument(s)]
None
[Return value]
List of action event information (see the ActionEventInfo class for detail)
[Detailed description]
- | This function displays information on the action event that has been set in the following format. |
action-event-number action-event-name state address string-to-be-attached-at-output variable-expression
|
action-event-number action-event-name state address Interrupt vector: interrupt-vector-number Priority level: interrupt-priority
|
[Example of use]
>>>ai = debugger.ActionEvent.Information()
1 Python Action Event0001 Enable main results: chData
2 Python Action Event0002 Disable sub Interrupt vector: 0x1c Priority level: 7
>>>print ai[0].Number
1
>>>print ai[0].Name
Python Action Event0001
>>>
|