debugger.DebugTool.Change
|
This function changes the debug tool.
[Specification format]
debugger.DebugTool.Change(debugTool)
|
[Argument(s)]
|
|
debugTool
|
Specify the debug tool to change.
The debug tools that can be specified are shown below.
|
|
|
DebugTool.Simulator
|
Simulator
|
DebugTool.Minicube
|
MINICUBE
|
DebugTool.Minicube2
|
MINICUBE2 (Serial connect)
|
DebugTool.Minicube2Jtag
|
MINICUBE2 (JTAG connect)
|
DebugTool.Iecube
|
IECUBE
|
DebugTool.Iecube2
|
IECUBE2
|
DebugTool.E1Jtag
|
E1 (JTAG connect)
|
DebugTool.E1Serial
|
E1 (Serial connect)
|
DebugTool.E1Lpd
|
E1 (LPD connect)
|
DebugTool.E2
|
E2 emulator (abbreviated name: E2)
|
DebugTool.E2Lite
|
E2 emulator Lite (abbreviated name: E2 Lite)
|
DebugTool.E20Jtag
|
E20 (JTAG connect)
|
DebugTool.E20Serial
|
E20 (Serial connect)
|
DebugTool.E20Lpd
|
E20 (LPD connect)
|
DebugTool.IE850A
|
IE850A
|
[Return value]
If the debug tool was changed successfully: True
If there was an error when changing the debug tool: False
[Detailed description]
- | This function changes the debug tool to the one specified by DebugTool.
However, the debug tool that can be changed differs depending on the using device. Select [Debug Tool] on the project tree and select [Using Debug Tool] on the context menu. And then confirm the debug tool that can be changed.
|
Caution | It is possible to specify non-selectable emulators. Only specify emulators that can be selected in CS+' s debugging tool. |
[Example of use]
>>>debugger.DebugTool.Change(DebugTool.Simulator)
True
>>>
|