debugger.SaveRegisterBank.Information


This function displays information on the save register bank. [RX]

[Specification format]

debugger.SaveRegisterBank.Information(bankNumberList = [])

[Argument(s)]

Argument

Description

bankNumberList

Specify the bank number of the banked register to display information (default: not specified).

When specifying multiple numbers, specify them by delimiting with a comma.

[Return value]

List of banked register information (see the BankedRegisterInfo property for detail)

[Detailed description]

-

This function displays information on the save register bank in the following format.

bank-number
register-name value

-

When bankNumberList is specified, information on the specified bank number.

-

When bankNumberList is not specified, then information on all banks will be displayed.

[Example of use]

>>> srb = debugger.SaveRegisterBank.Information([1, 3])
 
Save register bank 1
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
Save register bank 3
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
--------------
>>> print srb[0].BankNumber
1
>>> print srb[0].RegisterName
R1
>>> print srb[0].Value
0