debugger.Download.Property
|
This property sets or refers to conditions of the download file of the debug tool.
[Specification format]
debugger.Download.Property = downloadlist
|
[Setting(s)]
|
|
downloadlist
|
Set conditions of the download file of the debug tool as a list.
See the DownloadCondition class for details.
|
[Reference]
List of conditions of the download file
[Detailed description]
- | This property sets or refers to conditions of the download file of the debug tool. |
Caution | The list specified with downloadlist should be a C# list and not an IronPython list.
Therefore, first refer to the list of conditions and manipulate that list.
|
di = debugger.Download.Property
|
You can manipulate conditions in the list set for di.
For the usage, refer to [Example of use].
[Example of use]
>>>di = debugger.Download.Property
>>>print di[0].FileName
C:\project\test.abs
>>>print di[0].DownloadFileType
LoadModule
>>>dc = DownloadCondition()
>>>dc.FileName = "C:/project/test2.abs"
>>>dc.DownloadFileType = DownloadFileType.LoadModule
>>>di.Add(dc)
>>>debugger.Download.Property = di
>>>
|