debugger.SoftwareTraceLPD.RecordingMode


This property sets or refers to the operation of the debug tool when the memory for recording software trace information (LPD output) becomes full. [RH850][E2]

[Specification format]

debugger.SoftwareTraceLPD.RecordingMode = recordingMode

[Setting(s)]

Setting

Description

recordingMode

Set the operation of the debug tool when the memory for recording software trace information (LPD output) becomes full.

The values that can be specified are shown below.

Type

Description

TraceMode.FullBreak

Execution of the program and the writing of trace data stop when the recording memory is full.

TraceMode.FullStop

The writing of trace data stop when the recording memory is full.

TraceMode.NonStop

Trace data continue to be overwritten even after the recording memory is full.

[Reference]

The current setting for the operation of the debug tool when the memory for recording software trace information (LPD output) becomes full

[Detailed description]

-

This property sets or refers to the operation of the debug tool when the memory for recording software trace information (LPD output) becomes full.

[Example of use]

>>>print debugger.SoftwareTraceLPD.RecordingMode
NonStop
>>>debugger.SoftwareTraceLPD.RecordingMode = TraceMode.FullStop
>>>print debugger.SoftwareTraceLPD.RecordingMode
FullStop
>>>