![]()

2. Open the sample Project
In this step, you configure the information necessary to create a project.
|
In the "Load Sample Project" field, from the "RX" tab, select " RX65N_Tutorial_Basic_Operation", then click [GO]. |


|
Follow the on-screen instructions. A sample program opens as shown in the figure below. |