Starting CS+

3. Plug-in setting

In this tutorial, the Smart Configurator functions are not used.

If you want to use the Smart Configurator functions, please check the plug-in setting by following the below procedure.

Select [Plug-in Setting] from the [Tool] menu.

After configuring the settings as shown in the figure below, click [OK].

Select [Yes], then CS+ restarts.