2.7.9 Set the current build options as the standard for the project

On the build tool's Property panel, if you add a change to the settings for the standard build options, the value of the property will be displayed in boldface.

Figure 2.79

Property Panel (After Changing Standard Build Option)

 

To make the build options for the currently selected project (main project or subproject) the standard build options (remove the boldface), select the Build tool node on the project tree and select [Set to Default Build Option for Project] from the context menu.

Figure 2.80

[Set to Default Build Option for Project] Item

 

The values of the properties after setting them as the standard build option are as shown below.

Figure 2.81

Property Panel (After Setting Standard Build Option)

Caution

When the main project is selected, only the main project settings are made. Even if subprojects are added, their settings are not made.