2.7.8 Delete a build mode

Deleting a build mode is performed with the Build Mode Settings dialog box.

Select [Build Mode Settings...] from the [Build] menu. The dialog box will open.

Figure 2.77

Build Mode Settings Dialog Box

 

Select the build mode to be deleted from [Build mode list] and click the [Delete] button. The Message dialog box below will open.

Figure 2.78

Message Dialog Box

 

To continue with the operation, click the [OK] button in the dialog box.

The selected build mode is deleted from the project.

Caution 1.

You cannot delete "DefaultBuild".

Caution 2.

If the currently set build mode is deleted, "DefaultBuild" is set.