2.8.1 Run a build of updated files

Out of build target files, a build of only updated files is run (hereafter referred to as "build").

Running a build is performed for the entire project (main project and subprojects) or active project (see "2.7.5 Change the build target project").

(1)

When running a build of the entire project

Click on the toolbar.

(2)

When running a build of the active project

Select the project, and then select [Build active project] from the context menu.

Figure 2.85

[Build active project] Item

Remark

If the build of the included source file is not run after editing the header file and running the build, update the file dependencies (see "2.6.6 Update file dependencies").