2.8.2 Run a build of all files

A build of all build target files is run (hereafter referred to as "rebuild").

The cross reference file is deleted.

Running a rebuild is performed for the entire project (main project and subprojects) or active project (see "2.7.5 Change the build target project").

(1)

When running a rebuild of the entire project

Click on the toolbar.

(2)

When running a rebuild of the active project

Select the project, and then select [Rebuild active project] from the context menu.

Figure 2.86

[Rebuild active project] Item