2.8.3 Run a build in parallel with other operations

CS+ can automatically start a build when one of the following events occurs (hereafter referred to as "rapid build").

-

When any one of the following files that are added to the project is updated: (C source file, assembly source file, symbol address file, header file, object file, relocatable file, and library file)

-

When a build target file has been added to or removed from the project

-

When the link order of object module files and library files is changed

-

When the property of the build tool or build target file is changed

 

If a rapid build is enabled, it is possible to perform a build in parallel with the above operations.

To enable/disable a rapid build, select [Rapid Build] from the [Build] menu. A rapid build is enabled by default.

Figure 2.87

[Rapid Build] Item

 

Remark 1.

After editing source files, it is recommend to save frequently by pressing the [Ctrl] + [S] key.

Remark 2.

Enable/Disable setting of the rapid build applies to the entire project (main project and subprojects).

Remark 3.

If you disable a rapid build while it is running, it will be stopped at that time.

Caution

This function will also be enabled in an external text editor if the [Observe registered files changing] check box is selected in the [General - Build] category of the Option dialog box.