2.8.5
Compile/assemble individual files
You can just compile or assemble for each source file added to the project.
(1) | When compiling a C source file |
Select the C source file on the project tree and select the [Compile] from the context menu.
Figure 2.89 | [Compile] Item |
(2) | When assembling an assembly source file |
Select the assembly source file on the project tree and select the [Assemble] from the context menu.
Figure 2.90 | [Assemble] Item |