Changes the CPU clock/peripheral hardware clock.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_cgc.h”
MD_STATUS R_CGC_Set_ClockMode ( clock_mode_t mode );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       clock_mode_t mode;  | 
    
       Clock generator type HIOCLK : High-speed onchip oscillator SYSX1CLK : X1 clock SYSEXTCLK : External main system clock SUBXT1CLK : XT1 clock SUBEXTCLK : External subsystem clock  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ERROR1  | 
    
       Exit with error (abend)  | 
| 
       MD_ERROR2  | 
    
       Exit with error (abend)  | 
| 
       MD_ERROR3  | 
    
       Exit with error (abend)  | 
| 
       MD_ERROR4  | 
    
       Exit with error (abend)  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument specification  |