Usage example
Switch clock by external input.
[GUI setting example]
| 
       Clock Generator  | 
    
       Used  | |||
| 
       CGC  | 
    
       Used  | |||
| 
       Operation mode setting  | 
    
       High speed min mode 4.0(V) ≦ VDD ≦ 5.5(V)  | |||
| 
       Main system clock (fMAIN) setting  | 
    
       High-speed OCO(fIH)  | |||
| 
       fIH Operation  | 
    
       Used  | |||
| 
       fIH Frequency  | 
    
       64(MHz)  | |||
| 
       fMX Operation  | 
    
       Used  | |||
| 
       High-speed system clock setting  | 
    
       X1 oscillation(fX)  | |||
| 
       fMX frequency  | 
    
       4(MHz)  | |||
| 
       Stable time  | 
    
       65536 (2^18/fX) (μs)  | |||
| 
       fPLL operation  | 
    
       Unused  | |||
| 
       Main/PLL select clock (fMP) setting  | 
    
       64 (fMAIN)(MHz)  | |||
| 
       fSUB operation  | 
    
       Used  | |||
| 
       Subsystem clock (fSUB) setting  | 
    
       XT1oscillation(fXT)  | |||
| 
       fSUB frequency  | 
    
       32.768(kHz)  | |||
| 
       XT1 oscillator oscillation mode setting  | 
    
       Low power consumption  | |||
| 
       STOP  | 
    
       Subsystem clock in STOP, HALT mode setting  | |||
| 
       Internal low-speed oscillation clock (fIL) setting  | 
    
       15(kHz)  | |||
| 
       Low speed on-chip oscillatior clock (fSL) setting  | 
    
       32.768 (fSUB)(kHz)  | |||
| 
       WDT operation clock (fWDT) setting  | 
    
       15(kHz)  | |||
| 
       RTCoperation clock setting  | 
    
       32.768 (fSUB)(kHz)  | |||
| 
       Timer RD operation clock  | 
    
       64000 (fIH)(kHz)  | |||
| 
       CPU and peripheralclock setting (fCLK)  | 
    
       32000 (fMP/2) (kHz)  | |||
| 
       Interrupt  | 
    
       Used  | |||
| 
       INTP  | 
    
       Used  | |||
| 
       INTP0  | 
    ||||
| 
       Valid edge  | 
    
       Falling  | |||
| 
       Priority  | 
    
       Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Clear INTP0 interrupt flag and enable interrupt */
R_INTC0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_intc_user.c
/* Start user code for include. Do not edit comment generated here */
#include "r_cg_cgc.h"
/* End user code. Do not edit comment generated here */
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_cgc_f = 0U;
/* End user code. Do not edit comment generated here */
static void __near r_intc0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Change clock generator operation mode */
if (0U == g_cgc_f)
{
if (MD_OK == R_CGC_Set_ClockMode(SUBXT1CLK))
{
g_cgc_f = 1U;
}
}
else
{
if (MD_OK == R_CGC_Set_ClockMode(HIOCLK))
{
g_cgc_f = 0U;
}
}
/* End user code. Do not edit comment generated here */
}