Reads the counter value (year, month, weekday, day, hour, minute, second) of the real-time clock.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
MD_STATUS R_RTC_Get_CounterValue ( rtc_counter_value_t * const counter_read_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       rtc_counter_value_t * const counter_read_val;  | 
    
       Pointer to structure in which to store the counter value being read  | 
Remark See R_RTC_Set_CounterValue for details about the rtc_counter_value_t counter value.
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_BUSY1  | 
    
       Executing count process (before reading)  | 
| 
       MD_BUSY2  | 
    
       Stopping count process (after reading)  | 
Remark If MD_BUSY1 or MD_BUSY2 is returned, it may be because the counter-operation is stopped, or the counter operation start wait time is too short, so make the value of the RTC_WAITTIME macro defined in the header file "r_cg_rtc.h" larger.