Sets the alarm conditions (weekday, hour, minute).
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Set_AlarmValue ( rtc_alarm_value_t alarm_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       rtc_alarm_value_t alarm_val;  | 
    
       Alarm conditions (weekday, hour, minute)  | 
Remark Below is shown the structure rtc_alarm_value_t (alarm conditions).(The structure is different according to the device.)
| 
       typedef struct { uint8_t sec; /* Second */ uint8_t min; /* Minute */ uint8_t hour; /* Hour */ uint8_t week; /* Weekday (0: Sunday, 6: Saturday) */ uint8_t day; /* Day */ uint8_t month; /* Month */ uint16_t year; /* Year */ } rtc_alarm_value_t;  | 
- alarmws (Second)
Below are shown the meanings of each 
bit of the structure member alarmws.
- alarmwm (Minute)
Below are shown the meanings of each bit of the structure member alarmwm.
                     
- alarmwh (Hour)
Below are shown the meanings of each bit of the structure member alarmwh.
If the real-time clock is set to the 12-hour clock, then bit 5 has the following meaning.
0: AM
1: PM
                     
- alarmww (Weekday)
Below are shown the meanings of each bit of the structure member alarmww.
                     
- alarmwd (Day)
Below are shown the meanings of each bit of the structure member alarmwd.
                     
- alarmwmn (Month)
Below are shown the meanings of each bit of the structure member alarmwmn.
                     
- alarmwy (Year)
Below are shown the meanings of each bit of the structure member alarmwmn.
                     
[Return value]
None.