Everything
 

[Code Preview Information] tab (Product Information)


This tab allows you to view the information (Product Information) for the [Code Preview] selected in the Project Tree panel.

Figure A.7

[Code Preview Information] Tab (Product Information)

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview], and then select [Property] from the context menu.

Remark

If this panel is already open, selecting [Peripheral Functions] in the Project Tree panel changes the content displayed to that corresponding to the selected node.

[Description of each area]

(1)

[Product Information] category

This area allows you to view the information (Release Date and Version) for the [Code Preview] selected in the Project Tree panel.

Release Date

Displays the release date of the Code Generator (Design Tool).

Version

Displays the version number of the Code Generator (Design Tool).