This tab allows you to view the information (File Information) on and change the setting for the source code node selected in the Project Tree panel.
![](r20ut3104ej0110_cscgpf-51.gif)
The following items are explained here.
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview] >> Peripheral function node >> Source code node, and then select [Property] from the [View] menu. |
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview] >> Peripheral function node >> Source code node, and then select [Property] from the context menu. |
If this panel is already open, selecting the source code node in the Project Tree panel changes the content displayed to that corresponding to the selected node. |
This area allows you to view the information (Fine name, File used, Default name and Output folder) on and change the setting for the source code node selected in the Project Tree panel.
The name of the file can be changed by selecting [Rename] from the context menu after selecting the source code node in the Project Tree panel. |
||
Indicates whether or not output to a file is to proceed when the |
||
Selects whether or not to restore the default name of the file. Note that the default name of the file can be restored by selecting [Default] from the context menu after selecting the source code node in the Project Tree panel. |
||
Displays the output destination folder. Note that the output destination folder can be changed by using [Generate File Mode] >> [Output folder] in the [Code Generator Setting] tab. |