|
-END_RECORD [V1.05 or later]
|
This option specifies the end record.
[Specification format]
- | Interpretation when omitted |
The end record is output to suit the address of the entry point.
[Detailed description]
- | This option specifies the type of end record for a Motorola S-record file. |
- | The following can be specified for record. |
|
S7
|
S7 record
|
|
S8
|
S8 record
|
|
S9
|
S9 record
|
- | When the entry point address is larger than the specified address field, select an end record to suit the address of the entry point. |
[Example of use]
- | To output a 32-bit S-type end record regardless of the address range, write this as: |
> rlink a.obj b.obj -end_record=S7 -form=stype -output=c.mot
|
[Remark]
- | When -form={stype} is not specified, this option outputs an error message and terminates execution. |