|
-CFI_IGNORE_Module [Professional Edition only] [V1.06 or later] |
This option specifies object files to be exempted from the function list for use in detecting illegal indirect function calls.
-CFI_IGNORE_Module=suboption[, ...] [V1.06 or earlier] suboption := file [V1.07 or later] suboption := file[(module[, ...])] |
This option specifies object files to be exempted from the function list for use in detecting illegal indirect function calls.
[V1.07 or later]
This option specifies object files and library files to be exempted from the function list for use in detecting illegal indirect function calls. The module name in a library can be used to specify a library file.
For details on detecting illegal indirect function calls, refer to the item on the '-control_flow_integrity [Professional Edition only] [V1.06 or later]' compiler option.
If this option is specified more than once, the functions of all specified object files are exempted from the function list. |
When this option is used, the -CFI option must also be specified. If the -CFI option is not specified, an error will occur. |
To remove functions in the c module in the b.lib library from the function list, code as: