In the program execution process, the execution time in a section can be measured by setting Timer Result event.
To use this function, follow the procedure described below.
2.16.2.1 Set a Timer Result event
2.16.2.3 Edit a Timer Result event [Full-spec emulator][E1][E20]
2.16.2.4 Delete a Timer Result event
Also see "2.20.7 Notes for setting events" for details on Timer Result events (e.g. limits on the number of enabled events). |
To use this function, [Yes] must be specified with the [Use timer function] property in the [Timer] category on the [Debug Tool Settings] tab of the Property panel. |