You configure the flash self programming emulation (Code flash).
Note that this tab appears only when the selected microcontroller incorporates the flash memory.
(2) [Writing Time/Erasing Time]
(4) [Setting Flash shield window]
You can configure the flash self programming emulation function in this category.
![](Debug_RL78_E-17.gif)
Select whether to use the flash self programming emulation function.
Select [Yes] to use the flash self programming emulation function (default: [No]).
You can configure the delay time for writing to and erasing the flash memory in this category.
![](Debug_RL78_E-18.gif)
You can simulate the delay time for writing to the flash memory.
Select the value to simulate the delay time from the following drop-down list.
Specify the target address at which to simulate the delay time for writing.
Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0]).
Specify a mask value for the address for writing time.
Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0x3]).
The address for the writing time is masked bit-wise with a mask value for which "0" is specified.
The flash library writes to the code flash memory in 4-byte units, so fix the lowest and second-lowest order bits of the address mask to 1. |
To set an address for writing time between 0x1000 and 0x1FFF |
You can simulate the delay time for erasing the flash memory.
Select the value to simulate the delay time from the following drop-down list.
Specify the target address at which to simulate the delay time for erasing.
Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0]).
Specify a mask value for the address for erasing time.
Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0x3FF]).
The address for the writing time is masked bit-wise with a mask value for which "0" is specified.
The flash library erases the code flash memory in block units, so fix the lower-order 10 bits of the address mask to 1. |
To set an address for erasing time between 0x1000 and 0x1FFF |
In this category, you can configure the operation of flash functions in the self programming library, that are used for the flash macro service when performing the flash self programming.
![](Debug_RL78_E-19.gif)
Specify the error to generate in the flash macro service to emulate (errors will not be generated during normal emulation).
Three types of errors to generate ([0]/[1]/[2]) can be specified with subproperties for this property.
Select any one of the following types from each of the [Generate error] subproperties to return the error values forcibly.
1) Generate FlashErase Error (Erase)
2) Generate FlashBlankCheck Error (BlankCheck)
3) Generate FlashWrite Error (Write)
4) Generate FlashIVerify Error (IVerify)
5) Generate FlashSetSecurity / FlashSetFSW Error (Erase)
6) Generate FlashSetSecurity / FlashSetFSW Error (Write)
7) Generate FlashSetSecurity / FlashSetFSW Error (IVerify)
If you select one of 1) to 4), furthermore, specify the address within the flash memory and its mask valueNote at which the corresponding error is to be generated, with the [Address for error] and [Address mask value for error] subproperties that are listed newly in the lower area. Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0]).
When [Generate FlashWrite Error (Write)] is selected, fix the lowest and second-lowest order bits of the mask value to 1, because the flash library writes to the code flash memory in 4-byte units. |
You can specify the area that can be written or erased by flash self programming (Flash shield window function), in this category.
Settings of this category are applied after CPU reset is generated. |
![](Debug_RL78_E-20.gif)
Specify the start block of the area that can be written to and erased by flash self programming.
Directly enter the value in hexadecimal number from 0x0 to 0xFFFF (default: [0]).
Specify the end block of the area that can be written to and erased by flash self programming.
Directly enter the value in hexadecimal number from 0x0 to 0xFFFF (default: [FFFF]).
You can configure the function on the security flag emulation in this category.
The initial value of the security flag is emulated when the security has been set to the flash memory.
Settings of this category are applied after CPU reset is generated. |
![](Debug_RL78_E-21.gif)
Specify whether to emulate to disable block erase.
Select [Yes] to emulate to disable block erase (default: [No]).
Select whether to emulate to disable writing.
Select [Yes] to emulate to disable writing (default: [No]).
Select whether to emulate to disable rewrite boot area.
Select [Yes] to emulate to disable rewrite boot area (default: [No]).