You configure the data flash emulation function.
Note that this tab appears only when the selected microcontroller incorporates the data flash memory.
You can configure the data flash emulation function in this category.
![](Debug_RL78_E-22.gif)
Select whether to use the data flash emulation function.
Select [Yes] to use the data flash emulation function (default: [No]).
You can configure the delay time for writing to the data flash memory in this category.
![](Debug_RL78_E-23.gif)
You can simulate the delay time for writing to the data flash memory.
Select the value to simulate the delay time from the following drop-down list.
Specify the target address at which to simulate the delay time for writing.
Directly enter the address in hexadecimal number from 0xF1000 to 0xFFFFF (default: [F1000]).
Specify a mask value for the address for writing time.
Directly enter the address in hexadecimal number from 0x0 to 0xFFFFF (default: [0]).
The address for the writing time is masked bit-wise with a mask value for which "0" is specified.
To set an address for writing time between 0xF1000 and 0xF1FFF |
In this category, you can configure the operation of flash functions, that are used for the data flash macro service when performing the data flash emulation.
![](Debug_RL78_E-24.gif)
Specify the error to generate in the data flash macro service to emulate (errors will not be generated during normal emulation).
Four types of errors to generate ([0]/[1]/[2]/[3]) can be specified with subproperties for this property. Select any one of the following types from each of the [Generate error] subproperties to return the error values forcibly, and then specify the address within the data flash memory (0xF1000 to 0xFFFFF) and its mask value (0x0 to 0xFFFFF) at which the corresponding function error is to be generated, with the [Address for error] and [Address mask value for error] subproperties that are listed newly in the lower area.
[Address for error]: [F1000]/[Address mask value for error]: [0] is specified by default.
1) Generate write error for FlashWrite