The address condition and pass count condition [IECUBE][Simulator] for execution-related events you have set can be edited.
Perform this operation in the Detail dialog box (for execution events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an execution-related eventNote you want to edit on the Events panel.
An execution-related event refers to any one of the following events in the Events panel. |
Execution-related event as start and end condition in detailed information on Timer Result event [IECUBE][Simulator] |
![](Debug_RL78_E-381.gif)
You can edit the address condition for an execution-related event in this area.
![](Debug_RL78_E-382.gif)
![](Debug_RL78_E-383.gif)
![](Debug_RL78_E-384.gif)
From the [Compare condition] drop-down list, select the type of condition for address comparison.
After that, specify the address for use with the selected type of condition in the field displayed under the list.
It is possible to specify the value of an address mask for the specified address value [Simulator].
In this case, specify [Yes] in the [Use the address mask], and specify the mask value in the [Mask value] field under the list by directly entering a hexadecimal address.
In [Address], the address at which the execution-related event is currently set is displayed.
To edit this address, directly enter an address expression for the address value at which you want to set the event.
You can edit the pass count condition for an execution-related event in this area.
Directly enter a pass count value in decimal notation between 1 and 65535.
![](Debug_RL78_E-385.gif)