| 
 Detail dialog box (for execution events) 
 | 
This dialog box is used to display and modify detailed information on an execution-related event selected in the Events panel. 
Note that the execution-related events refer to the following events in the Events panel.
-  | Hardware Break event (execution type)  | 
 
-  | Execution-related break event in detailed information on Combination Break event [E1][E20]  | 
 
-  | Execution-related event as start and end condition in detailed information on Trace event  | 
 
-  | Execution-related event as start and end condition in detailed information on Timer Result event [IECUBE][Simulator]  | 
 
Figure A.33  | Detail Dialog Box (for Execution Events) [IECUBE]  | 
 
Figure A.34  | Detail Dialog Box (for Execution Events) [E1][E20][EZ Emulator]  | 
 
Figure A.35  | Detail Dialog Box (for Execution Events) [Simulator]  | 
 
 
This section describes the following.
[How to open]
-  | On the Events panel, move the caret to any one of the following events, and then select [Edit Condition...] from the context menu.  | 
 
-  | Hardware Break event (execution type)  | 
 
-  | Execution-related break event in detailed information on Combination Break event [E1][E20]  | 
 
-  | Execution-related event as start and end condition in detailed information on Trace event  | 
 
-  | Execution-related event as start and end condition in detailed information on Timer Result event [IECUBE][Simulator]  | 
 
[Description of each area]
(1)  | Event conditions setting area  | 
 
Specify the address condition.
| 
 
Compare condition 
[IECUBE] 
[Simulator] 
 | 
 
Specify the condition to compare address. 
 | 
| 
 
Default 
 | 
 
Specified address (==) 
 | 
| 
 
Modifying 
 | 
 
Select from the drop-down list 
 | 
| 
 
Available values 
 | 
 
Specified address (==) 
 | 
 
Specifies the address with [Address]. 
 | 
| 
 
Greater than or equal to (>=) 
 | 
| 
 
Less than or equal to (<=) 
 | 
| 
 
Inside the range (<=Values<=) 
 | 
 
Specifies the range with [Start address] and [End address]. 
 | 
| 
 
Outside the range !(<=Values<=) 
 | 
| 
 
Address 
  
 | 
 
Specify the address. 
[IECUBE][Simulator] 
This item appears only when [Specified address (==)], [Greater than or equal to (>=)] or [Less than or equal to (<=)] is selected in [Compare condition]. 
 | 
| 
 
Default 
 | 
 
The current set value 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard. 
 | 
| 
 
Available values 
 | 
 
Address expression within the valid range 
 | 
| 
 
Start address 
[IECUBE] 
[Simulator] 
 | 
 
Specify the start address.  
[IECUBE][Simulator] 
This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. 
 | 
| 
 
Default 
 | 
 
The current set value 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard. 
 | 
| 
 
Available values 
 | 
 
Address expression within the valid range 
 | 
| 
 
End address 
[IECUBE] 
[Simulator] 
 | 
 
Specify the end address.  
[IECUBE][Simulator] 
This item appears only when [Inside the range (<=Values<=)] or [Outside the range !(<=Values<=)] is selected in [Compare condition]. 
 | 
| 
 
Default 
 | 
 
The current set value 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard. 
 | 
| 
 
Available values 
 | 
 
Address expression within the valid range 
 | 
| 
 
Use the address mask 
[Simulator] 
  
 | 
 
Specify whether to specify an address mask. 
 | 
| 
 
Default 
 | 
 
No 
 | 
| 
 
Modifying 
 | 
 
Select from the drop-down list 
 | 
| 
 
Available values 
 | 
 
Yes 
 | 
 
Specifies an address mask. 
 | 
| 
 
No 
 | 
 
Does not specify an address mask. 
 | 
| 
 
Mask value 
[Simulator] 
  
 | 
 
Specify the value of address mask. 
This item appears only when [Use the address mask] is set to [Yes]. 
 | 
| 
 
Default 
 | 
 
The current set value 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard. 
 | 
| 
 
Available values 
 | 
 
Hexadecimal number up to five digits 
 | 
 
(b)  | [Pass Count] [IECUBE][Simulator]  | 
 
Specify the pass count condition. 
| 
 
Pass count 
  
 | 
 
Specify a pass count. 
The relevant event occurs when the event condition is met as many times as the specified pass count. 
 | 
| 
 
Default 
 | 
 
1 
 | 
| 
 
Modifying 
 | 
 
Directly enter from the keyboard. 
 | 
| 
 
Available values 
 | 
 
1 to 65535 in decimal number 
 | 
 
Caution  | [IECUBE] 
A value other than "1" cannot be specified as the pass count condition for an execution-related event (before execution).   | 
 
This area displays a simple description of the item selected in the Event conditions setting area. 
[Toolbar]
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Applies detailed settings made in this dialog box to execution-related events and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Cancels the save and closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box. 
 |