Everything
 

Parts List dialog box


This dialog box displays all the figure objects created in the I/O Panel window as well as the pin connection status of part objects.

The pin connection settings for each object can be changed in the property dialog box, which can be opened by double-clicking the relevant object listed in this dialog box, or selecting the relevant object listed in this dialog box and then selecting the [View] menu >> [Properties...].

Figure A.88

Parts List Dialog Box

 

This section describes the following.

[How to open]

-

With the I/O Panel window in focus, select [Parts List...] form the [View] menu.

[Description of each area]

(1)

Pin connection status display area

Label

Displays the label (name) attached to the object. Nothing is displayed for objects that do not have a label.

Parts

Displays the part category.

rectangle

Straight line, rectangle, ellipse, rounded rectangle, fan shape

polygon

Polygon

text

Text

bitmap

Bitmap

button

Push button, pull button, group button

analog button

Analog button

key

Key matrix

level gauge

Level gauge

led

LED

7segment led

7-segment LED

14segment led

14-segment LED

matrix led

Matrix LED

buzzer

Buzzer

groups

Grouped part

Pin Name

Displays the pins connected to parts.

"-" is displayed for parts that are connected to multiple pins, and a blank is displayed for parts that are unconnected.

Active Level

Displays the active value set for the part.

"-" is displayed for parts that are connected to multiple pins, and a blank is displayed for parts that are unconnected.

[Function buttons]

Button

Function

Close

Closes the this dialog box.