This dialog box is used to set the serial format for the asynchronous serial interface (UART).
![](Debug_RL78_E-1021.gif)
This section describes the following.
On the Serial window with the UART serial interface, any one of the following:
Directly input the serial baud rate value as an integer. (Unit: bps) |
||
Select the bit length of the transmission data from the drop-down list, or specify it through direct input (default:7). |
||
Select the stop bit length from the drop-down list (default:1). |
||
Select the parity information (none parity (default) /odd parity/even parity/0 parity). |
||
Select this item to repeat data transfer when the [Auto Send] button in the Serial window has been clicked. |
||
Following transmission of the last data during automatic transmission, returns to the beginning of the data and performs automatic transmission. |
||
Following transmission of the last data during automatic transmission, stops transmission (default). |